Freescale imx25 demo image ts_calibration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale imx25 demo image ts_calibration problem

ソリューションへジャンプ
2,171件の閲覧回数
gurumoorthirasi
Contributor IV

Dear imx community,

I have tried with demo image with imx25 board for ts_calibration to check my board touchscreen functionality is working or not.

while booting up the demo image during the boot process it will ask the user to touch the screen for touch screen calibration even i touched that there is no response from screen on terminal

the terminal message is like  and also gnome desktop is not coming on screen.  please give the soltion to resolve this issue.

i cant get the freescale login also . it is like below in terminal...

-------      

xres = 640, yres = 480                                                                                               
Failed to get root pixmap id                                                                                         
matchbox-panel: creating //.matchbox directory for session files                                                     
matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None )                                      
matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( None )                                 
user_overides is (nil)                                                                                               
mb-desktop-dotdesktop: failed to open /usr/local/share/applications                                                  
mb-desktop-dotdesktop: failed to open //.applications                                                                
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name                                             
mb-applet-menu-launcher: failed to open /usr/local/share/applications                                                
mb-applet-menu-launcher: failed to open //.applications                                                              
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name                                             
mb-applet-menu-launcher: failed to open /usr/local/share/applications                                                

mb-applet-menu-launcher: failed to open //.applications

---------

Regards,

Guru

ラベル(2)
0 件の賞賛
返信
1 解決策
1,836件の閲覧回数
gurumoorthirasi
Contributor IV

Yixing, Thank you for tracking this issue. the problem has been solved . the problem is in connector.there is some lose contact.

Regards,

Guru

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,836件の閲覧回数
YixingKong
Senior Contributor IV

Guru, our engineer is contacting you and asking you question. please respond to the question as soon as possible. If your issue had been resolved or no long exists, please click Correct Answer/Helpful Answer in 3 days.

Thanks,

Yixiing

1,837件の閲覧回数
gurumoorthirasi
Contributor IV

Yixing, Thank you for tracking this issue. the problem has been solved . the problem is in connector.there is some lose contact.

Regards,

Guru

0 件の賞賛
返信
1,836件の閲覧回数
maheshmahadeva1
NXP Employee
NXP Employee

Have you tried hitting the carriage return on the terminal.

Best regards,

-Mahesh