Freescale i.MX6Q Linux window frame has steps when quickly moving it in X-window after install X11 GFX HW acceleration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale i.MX6Q Linux window frame has steps when quickly moving it in X-window after install X11 GFX HW acceleration

2,183 Views
m_c
Senior Contributor I

The window frame has steps when move it even we installed Freescale's X-window driver "gpu-viv-bin-mx6q_3.0.35-4.1.0_armel.deb" already.

How customer make sure whether the gpu H/W acceleration is enabled properly? ex: to check /var/log/Xorg.0.log? or something else we can check?

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

2,059 Views
OtavioSalvador
Senior Contributor II

I strongly advise you to use the last Yocto Project-based builds. We have some machines with images ready for use online[1] and you might want to try the fsl-image-multimedia

1. Public images - fsl-community-bsp/dizzy/

0 Kudos
Reply