Freescale base distro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale base distro

1,211 Views
shanerogers
Contributor I

Hi, can anyone tell me what distro Freescale Linux is built/based on?

I'm new to this community, so please forgive me if I am asking in the wrong forum or doing something equally noobian.

0 Kudos
Reply
1 Reply

1,133 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use BSP documentation for the recent release for more details about NXP / FSL Linux bsp

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&Parent_nodeId=13376994810717061...

Summary page :

i.MX 6 Series Software and Development Tool|NXP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply