Freescale Linux 2.6-imx.git Fatal Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale Linux 2.6-imx.git Fatal Error

1,740 Views
ThanarajS
Contributor III

Hi All,

We are trying to git freescale linux-imx.git code but we were not able to download the kernel code for Android 7.

Is there any server issue in Freescale linux-imx?

Last Two days we are getting below error,

root@cpu-493-PC:/work/myandroid# git clone git://git.freescale.com/imx/linux-imx.git kernel_imx
Cloning into 'kernel_imx'...
fatal: repository 'https://git.freescale.com/imx/linux-imx.git/' not found


root@cpu-493-PC:/work/myandroid# git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx
Cloning into 'kernel_imx'...
fatal: repository 'https://git.freescale.com/imx/linux-2.6-imx.git/' not found
root@cpu-493-PC:/work/myandroid#

Thanks

Regards,

Raj.

Regards,
Thanaraj Subramani
Labels (5)
0 Kudos
Reply
2 Replies

1,444 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi, we are working internally to get this resolved.   The GIT managers are aware of the issue and we are working to find the root cause and solution.  In the meantime, you can navigate to the GIT website in web browser and download packages from there.   We hope to have it resolved soon.


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,444 Views
ko-hey
Senior Contributor II

Hi @Carlos_Musich

I had a same problem now.

Have it already resolved ?

Ko-hey

0 Kudos
Reply