Freescale IMX6 cortex A9 1GHZ RTC consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale IMX6 cortex A9 1GHZ RTC consumption

1,988件の閲覧回数
neerajchhabra
Contributor I

Hi, I am using Congatec QMX6 module which has Freescale IMX6 cortex A9 1GHZ single core processor. I want to provide a coin cell for the RTC backup so what would be the current consumption for the RTC? As stated by congatec it is 1.45UA at 20 degC and by freescale datasheet it is 41UA. Please help me to calculate proper consumption.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,711件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Neeraj

typical value is 15-20uA, however at high

temperature limit it may be as given in

IMX6DQCEC Table 8. Maximum Supply Currents.

It can not be calculated/predicted by any formula.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,711件の閲覧回数
neerajchhabra
Contributor I

Hi Igor,

I am confused which value I will take. In Table 8 for

VDD_SNVS_IN

, it is 275uA under normal conditions?

0 件の賞賛
返信

1,711件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Neeraj

this is at high temperature limit (95C for

Standard Consumer ).

0 件の賞賛
返信