Freeing memory after glTexDirectVIVMap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freeing memory after glTexDirectVIVMap

2,167件の閲覧回数
gsoft
Contributor I

Hi all,

I am using an iMX6.Quad

I need to load quickly some 2048x2048 textures into the GPU Mem and the glTexDirectVIVMap extension is perfect for this purpose (Note: once in the GPU Mem, those textures do not need some refresh).

I am not sure about how to release the memory.

What am I doing is:

uchar* pData = new uchar[memsize]; //pData is 64bits aligned

GLuint iPhysical = ~0U;

[...] // Filling pData with some data

glGenTextures(1, &iTex);

glBindTexture(GL_TEXTURE_2D, iTex);

glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MAG_FILTER, GL_LINEAR);

glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_MIN_FILTER, GL_LINEAR);

glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_WRAP_S, GL_CLAMP_TO_EDGE);

glTexParameteri(GL_TEXTURE_2D, GL_TEXTURE_WRAP_T, GL_CLAMP_TO_EDGE);

glTexDirectVIVMap(GL_TEXTURE_2D, 2048, 2048, GL_VIV_UYVY, (GLvoid**)&pData, &iPhysical);

glTexDirectInvalidateVIV(GL_TEXTURE_2D);

[...] // Using the texture with some GL instructions

 

It is working pretty well.

When the texture need to be released, I am just deleting it with: delete[] pData.

The question is:

Do I need to call glDeleteTextures(1, &iTex) to tell the GLES2 engine that the texture does not exist anymore? Or How can I be sure that the GPU wont use this shared memory space anymore?

Since I am using glTexDirectVIVMap, instead of glTexImage2D, my app crash because of the memory used.

Thank you for your help.

Fabien

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,925件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Fabien,

I guess this going to help you.

https://community.nxp.com/thread/433086 

0 件の賞賛
返信

1,925件の閲覧回数
gsoft
Contributor I

Hi,

Thank you for your reply. Yes indeed, the crash seems to be related with the memory leak of the 3.0.35. We are currently patching our kernel to check if the problem is fixed.

Beyond the memory leak, what is the best way to release the memory after a glTexDirectVIVMAP? Should the memory be released with glDeleteTexures or with delete [] or with both?

Fabien

0 件の賞賛
返信