Framebuffer support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Framebuffer support

1,663件の閲覧回数
jonver
Contributor II

Hi,

Is there any decent manual available on how to add framebuffer support on the imx6(ul)?

I suppose I need to make changes in the following:

1) Kernel modules

2) Device tree

3) U-Boot bootargs

I've build my kernel with the following modules

FB_TFT=y

CONFIG_FB_TFT_ILI9325=m

I added the following to the device tree

  1. / {
  2.      itdb28 {
  3.         compatible = "ilitek,ili9325";
  4.         status = "okay";
  5.  
  6.         rotate = <0>;
  7.         bgr;
  8.         buswidth = <8>;
  9.         reset-gpios = <&gpio3 23 0>;
  10.         dc-gpios = <&gpio3  5 0>;
  11.         cs-gpios = <&gpio3  1 0>;
  12.         wr-gpios = <&gpio3  0 0>;
  13.         db-gpios = <&gpio3  7 0>,
  14.                <&gpio3  8 0>,
  15.                <&gpio3  9 0>,
  16.                <&gpio3 10 0>,
  17.                <&gpio3 11 0>,
  18.                <&gpio3 15 0>,
  19.                <&gpio3 16 0>,
  20.                <&gpio3 17 0>;
  21.         /* LED pin drives backlight directly. Use transistor (50mA) */
  22.         /* led-gpios = <&gpio 4 1>; */
  23.         debug = <7>;
  24.     };
  25.  
  26.  
  27.     framebuffer {
  28.         compatible = "simple-framebuffer";
  29.         reg = <0x1d385000 (240 * 320 * 2)>;
  30.         width = <240>;
  31.         height = <320>;
  32.         stride = <(240 * 2)>;
  33.         format = "r5g6b5";
  34.     };
  35. };

Which provides me the following error:

Error opening /dev/fb0: No such file or directory

Thanks!

ラベル(4)
0 件の賞賛
返信
1 返信

1,454件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

0 件の賞賛
返信