Framebuffer bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Framebuffer bug

2,087件の閲覧回数
dmitriipetrov
Contributor I

I think, that's something wrong with my SABREAI board.

I just built AOSP following instructions from Android User's Guide.

I think, that something is wrong with configuration or with AOSP code.

There are too many messages like this one:

dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

Full log:

01-01 00:12:18.341 2754-2773/? D/Index: Locale 'en_AU' is already indexed

01-01 00:12:18.405 196-1251/? E/BufferQueueProducer: [StatusBar] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

01-01 00:12:18.489 2754-2774/? D/OpenGLRenderer: Render dirty regions requested: true

01-01 00:12:18.528 2754-2754/? D/Atlas: Validating map...

01-01 00:12:18.708 2754-2769/? W/art: Suspending all threads took: 10.968ms

01-01 00:12:18.722 2754-2769/? I/art: Background partial concurrent mark sweep GC freed 1542(131KB) AllocSpace objects, 1(16KB) LOS objects, 51% free, 948KB/1972KB, paused 15.127ms total 68.113ms

01-01 00:12:19.305 2754-2754/? D/DashboardSummary: rebuildUI took: 727 ms

01-01 00:12:19.314 2754-2754/? I/Choreographer: Skipped 46 frames!  The application may be doing too much work on its main thread.

01-01 00:12:19.706 2754-2774/? D/libEGL: loaded /system/lib/egl/libEGL_VIVANTE.so

01-01 00:12:19.735 2754-2774/? D/libEGL: loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

01-01 00:12:20.090 2754-2774/? D/libEGL: loaded /system/lib/egl/libGLESv2_VIVANTE.so

01-01 00:12:20.320 1348-1628/? W/audio_hw_primary: do_out_standby... 1979414272

01-01 00:12:20.358 2754-2774/? I/OpenGLRenderer: Initialized EGL, version 1.4

01-01 00:12:20.376 2754-2774/? D/OpenGLRenderer: Enabling debug mode 0

01-01 00:12:20.474 196-466/? E/BufferQueueProducer: [com.android.settings/com.android.settings.Settings] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

01-01 00:12:20.808 2754-2754/? I/Choreographer: Skipped 84 frames!  The application may be doing too much work on its main thread.

01-01 00:12:21.329 1586-1610/? I/ActivityManager: Displayed com.android.settings/.Settings: +4s69ms

01-01 00:12:21.516 2754-2754/? I/Choreographer: Skipped 41 frames!  The application may be doing too much work on its main thread.

ラベル(5)
0 件の賞賛
返信
1 返信

1,586件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Dmitri,

Can you please share the Android BSP  version that you are using????,   We need to have the version of the GPU driver. In order to move forward.

0 件の賞賛
返信