Frame Buffer sharing between HDMI and LCD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Frame Buffer sharing between HDMI and LCD

3,795 次查看
Subodh_K
Contributor I

Hi all,

I am working on a project which is based on IMX6Q board.I have integrated LCD and HDMI module to it and enabled hot pluggable support in kernel .

My LCD is connected on parallel port and HDMI is based on I2C. I am using frame buffer mxcfb1 for HDMI and for LCD is mxcfb2. Individually working fine

both LCD and HDMI.But when i give the mxcfb2 frame buffer in U-BOOT arguments but it does not seem working.

$ editenv mmcargs

Added This line

video=mxcfb2:dev=lcd,480x272@60,if=RGB24 video=mxcfb2:dev=hdmi,1920x1080M@60,if=RGB24

$ saveenv

$boot

It does not come on any display (LCD and HDMI).




If i try with their individual frame buffer in that case only LCD work not an HDMI.

video=mxcfb2:dev=lcd,480x272@60,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24

Please help me to debug this issue soon.

0 项奖励
回复
4 回复数

2,973 次查看
joanxie
NXP TechSupport
NXP TechSupport

you said: "I am using frame buffer mxcfb1 for HDMI and for LCD is mxcfb2. Individually working fineboth LCD and HDMI." and "

If i try with their individual frame buffer in that case only LCD work not an HDMI.

video=mxcfb2:dev=lcd,480x272@60,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24

"

any typo? when you set mxcfb1 to hdmi and mxcfb2 to lcd, ok or not?

0 项奖励
回复

2,973 次查看
Subodh_K
Contributor I

Hi Guanqiong ,

There is no typo in bootargs  i checked it many times .

0 项奖励
回复

2,973 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you mean when you can use this two commans 1)video=mxcfb2:dev=lcd,480x272@60,if=RGB24 2)video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24 Individually, but when you use together, just lcd is ok, right?

1) pls ensure you use different IPU or different port of same IPU

2) try to use the command video=mxcfb0:dev=lcd,480x272@60,if=RGB24 bpp=32

video=mxcfb1:dev=hdmi, 1920x1080M@60, if=RGB24 bpp=32

video=mxcfb2:off fbmem=5M,28M

3) when the board bootup, use the command "echo "0" >/sys/class/graphics/fb2/blank"

0 项奖励
回复

2,973 次查看
Subodh_K
Contributor I

Hi Guanqiong,

I am using kernel 3.10.17 which has device tree concept and i have changed according to my need .

In LCD I am using mxcfb2 framebuffer:

mxcfb3: fb@2 {

                compatible = "fsl,mxc_sdc_fb";

                disp_dev = "lcd";

                interface_pix_fmt = "RGB24";

                mode_str ="CLAA-WVGA";

                default_bpp = <16>;

                int_clk = <0>;

                late_init = <0>;

                status = "okay";

        };

For HDMI i am using mxcfb1 :

  mxcfb2: fb@1 {

                compatible = "fsl,mxc_sdc_fb";

                disp_dev = "hdmi";

                interface_pix_fmt = "RGB24";

                mode_str ="1920x1080M@60";

                default_bpp = <24>;

                int_clk = <0>;

                late_init = <0>;

                status = "okay";

        };

For IPU and Device ID assignment in LCD case :

  lcd@0 {

                compatible = "fsl,lcd";

                ipu_id = <0>;

                disp_id = <0>;

                default_ifmt = "RGB24";

                pinctrl-names = "default";

                pinctrl-0 = <&pinctrl_ipu1_1>;

                status = "okay";

        };

For IPU and Device ID assignment in case of HDMI:

&hdmi_core {

        ipu_id = <0>;

        disp_id = <1>;

        status = "okay";

};

And for blanking if i use echo 1 > /sys/class/graphics/fb0/blank  it controls both display.

0 项奖励
回复