For the IMX6 series of chip enable_wait_mode=off, I do not know what effect the wait_mode can have after it has been enabled. The corresponding instructions are not found in the manual.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For the IMX6 series of chip enable_wait_mode=off, I do not know what effect the wait_mode can have after it has been enabled. The corresponding instructions are not found in the manual.

1,313 Views
chenzongcha
Contributor I

For the IMX6 series of chip enable_wait_mode=off, I do not know what effect the wait_mode can have after it has been enabled. The corresponding instructions are not found in the manual.

0 Kudos
Reply
1 Reply

1,087 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Wait mode was concerned with the following bug in old Linux BSP releases: 
"System will not boot up successfully on the pre-production chip such as the
TO1.1/TO1.0 chip."  Hardly customers use such pre-productions parts now.
NXP decided to drop the preproduction (TO1.1/TO1.0) chip support. Customers
should use the production chip.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply