For increasing the capacity of RTC backup battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For increasing the capacity of RTC backup battery

Jump to solution
3,413 Views
george
Senior Contributor II

Dear all,

We use i.MX6 for industrial equipment.

The equipment needs RTC.

It has usually stopped for a long time in many cases.

Therefore, in order to keep RTC operation for a long time, it must have a large capacity backup battery.

We use MMPF0100 with i.MX6.

However, the current which can be supplied from MMPF0100 for LICELL charge is 60uA.

Therefore, the charge for the large capacity LICELL cannot be finished within the equipment operation period.

We will change the i.MX6-SDP schematics to which it refers, in order to remove 60uA limitation.

It gets the charging current from GEN_3V3.

Is our schematics available as the file attached here?

Is there any point which takes care?

Best Regards,

George

Labels (1)
0 Kudos
Reply
1 Solution
3,135 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

I looked at attached here picture

and think that such solution is quite feasible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,136 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

I looked at attached here picture

and think that such solution is quite feasible.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,135 Views
george
Senior Contributor II

Dear Igor,

THX

BR,

George

0 Kudos
Reply