For DDR Memory word size 64 bits, which clock is connected upper 32 bits and which clock is connected lower 32 bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For DDR Memory word size 64 bits, which clock is connected upper 32 bits and which clock is connected lower 32 bits

1,412 Views
muralikrishna
Contributor I


Hi All,

we need to achieve 64 bits word size. we are using 4 memory chips of 256MX16.

i.MX6 processor is generating two pairs of differentail clocks.

out of two pairs generated by processor which pair of the clock we need to connected Memory chips and what is the purpose of two pairs of differentail clocks.

Labels (1)
0 Kudos
Reply
1 Reply

1,312 Views
Yuri
NXP Employee
NXP Employee

As for DRAM clocks : in default state both signals are the same and can be used for both (any)

CS0 or CS1 if this makes easier PCB design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply