For DDR Memory word size 64 bits, which clock is connected upper 32 bits and which clock is connected lower 32 bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For DDR Memory word size 64 bits, which clock is connected upper 32 bits and which clock is connected lower 32 bits

1,401件の閲覧回数
muralikrishna
Contributor I


Hi All,

we need to achieve 64 bits word size. we are using 4 memory chips of 256MX16.

i.MX6 processor is generating two pairs of differentail clocks.

out of two pairs generated by processor which pair of the clock we need to connected Memory chips and what is the purpose of two pairs of differentail clocks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,301件の閲覧回数
Yuri
NXP Employee
NXP Employee

As for DRAM clocks : in default state both signals are the same and can be used for both (any)

CS0 or CS1 if this makes easier PCB design.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信