Flexspi driver SDK for nonblocking mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexspi driver SDK for nonblocking mode

2,205 Views
Sridharanblr
Contributor I

Hi ,

We are working on Flexspi drivers for our internal project, As part of this I wanted to develop driver in TransferNonBlock mode, 

We did not find a SDK for this in below SDK folder. 

SDK_2.5.1_MIMXRT1052xxxxB\microll_imxrt1052\SDK_2.5.1_MIMXRT1052xxxxB\boards\evkbimxrt1050\driver_examples

Can I get the sample code to Test Eval board on non blocking mode. Currently I can see the example is for polling 

0 Kudos
Reply
4 Replies

2,201 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sridharan

 

for TransferNonBlock mode one can look at MCUXpresso documentation

https://mcuxpresso.nxp.com/api_doc/dev/1315/group__flexspi.html

 

Best regards
igor

 

0 Kudos
Reply

2,199 Views
Sridharanblr
Contributor I

Hi ,

I have this info, I need a working code which I can port to our architecture. Pl provide an example code. 

Thanks 

 

0 Kudos
Reply

2,193 Views
igorpadykov
NXP Employee
NXP Employee

example was sent via mail.

 

Best regards
igor

0 Kudos
Reply

1,997 Views
Ykciv
Contributor III

Can I get the example code please? Im also trying to use non blocking method.

0 Kudos
Reply