FlexRAM OCRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexRAM OCRAM

1,924 次查看
po-pony
Contributor II

It is stated in the application note - AN12077, that the minimum configuration of OCRAM is 64 KB. This is
required due to ROM code requires at least 64 KB of RAM for its execution. The minimum OCRAM requirements can be device dependent.

But I can't find any such description in the 1024/1050 reference manual. All described are “RAM size of ITCM, DTCM and OCRAM can be configured from 0 to full RAM Array size separately".

I set OCRAM to 0, and the code seems to be able to run, so what is the actual situation?

0 项奖励
回复
2 回复数

1,912 次查看
Yuri
NXP Employee
NXP Employee

@po-pony 
Hello,
 

  Some memory is needed for boot purposes, therefore - although FlexRAM can be configured
for any size, including zero - really the minimum configuration of OCRAM of 64 KB is required
by boot ROM - this is correct. This relates only to boot ROM, which is affected only by
the FUSE FlexRAM bank configuration.

Regards,
Yuri.

 

0 项奖励
回复

1,896 次查看
po-pony
Contributor II

Thank you!