FlexCAN transceivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN transceivers

3,458件の閲覧回数
kishorekrish
Contributor I

HI,

I want to implement CAN node for that i have IMX6Q6AVT  soc. I think it already have a FlexCAN controller then i need a CAN transceiver.  so please let me know what are the various types of CAN transceivers supported by your FlexCAN controller,

If any transceiver is support then let me know is driver required for that transceiver or not ???@

Thank you.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

3,009件の閲覧回数
art
NXP Employee
NXP Employee

All common types of CAN transceivers are supported. The most popular and widespread ones seem to be the TJA1050 series transceivers by NXP:

TJA1050|NXP

They do not require any additional software drivers.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,004件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The SABRE_AI_DESIGNFILES board support the CAN module you can refer to it. And here I share a document about the CAN work on our i.MX6Q SabreSD. Hope it can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信