Flashloader for i.MXRT1160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashloader for i.MXRT1160

ソリューションへジャンプ
1,807件の閲覧回数
vishnusudhankj
Contributor III

Hi,

Where can I find the FlashLoader for i.MXRT 1160 platform.

For 1060 i can able to download through Flash loader i.MXRT1060 (nxp.com),

But for i.MXRT1160 , could not able to locate the FlashLoader?

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,793件の閲覧回数
jay_heng
NXP Employee
NXP Employee

flashloader will not be standalone release any more, it is included in SDK

When you build SDK from https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK, you need to check MCU Boot middleware

RT1160_SDK.PNG

Then you can find flashloader project at \SDK_2.12.0_MIMXRT1160-EVK\boards\evkmimxrt1160\bootloader_examples\flashloader

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,794件の閲覧回数
jay_heng
NXP Employee
NXP Employee

flashloader will not be standalone release any more, it is included in SDK

When you build SDK from https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK, you need to check MCU Boot middleware

RT1160_SDK.PNG

Then you can find flashloader project at \SDK_2.12.0_MIMXRT1160-EVK\boards\evkmimxrt1160\bootloader_examples\flashloader

 

0 件の賞賛
返信
1,801件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

Unlike the RT10XX, the RT11XX flashloader is located at the SDK.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信