Flashloader for i.MXRT1160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashloader for i.MXRT1160

Jump to solution
1,808 Views
vishnusudhankj
Contributor III

Hi,

Where can I find the FlashLoader for i.MXRT 1160 platform.

For 1060 i can able to download through Flash loader i.MXRT1060 (nxp.com),

But for i.MXRT1160 , could not able to locate the FlashLoader?

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,794 Views
jay_heng
NXP Employee
NXP Employee

flashloader will not be standalone release any more, it is included in SDK

When you build SDK from https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK, you need to check MCU Boot middleware

RT1160_SDK.PNG

Then you can find flashloader project at \SDK_2.12.0_MIMXRT1160-EVK\boards\evkmimxrt1160\bootloader_examples\flashloader

 

View solution in original post

0 Kudos
Reply
2 Replies
1,795 Views
jay_heng
NXP Employee
NXP Employee

flashloader will not be standalone release any more, it is included in SDK

When you build SDK from https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK, you need to check MCU Boot middleware

RT1160_SDK.PNG

Then you can find flashloader project at \SDK_2.12.0_MIMXRT1160-EVK\boards\evkmimxrt1160\bootloader_examples\flashloader

 

0 Kudos
Reply
1,802 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

Unlike the RT10XX, the RT11XX flashloader is located at the SDK.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply