Flashing through a HUB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing through a HUB

2,249 Views
puneethkumar
Contributor III

Dear Team,

I am using i.MX8DXL for my design, below are the queries i am having

a) CPU supports two USB2.0 - In between the two which one i can select for flashing 

b) I want USB2.0 for one of Module , can i mux another USB2.0 for flashing & another Module. - like using a USB2.0 2 port HUB - One for flashing other for one module.

 

 

0 Kudos
Reply
4 Replies

2,238 Views
puneethkumar
Contributor III

Yes  I was referring to i.MX8DX

 

0 Kudos
Reply

2,231 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The module should be connected to the hub, OTG as a separate burner

2021-04-21 163534.jpg

0 Kudos
Reply

2,236 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I do not think you can do that:

For the OTG core, there is only one port.
The port can be used as either a downstream or an upstream port.

usb2.0.PNG

0 Kudos
Reply

2,239 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you mean i.MX8DX or could you give us your product part number?

0 Kudos
Reply