Hello NXP TechSupport
I built the version imx-5.4.3-1.0.0 on imx8qmmek,but I got different version image.
I followed these following build steps on Ubuntu16.04, and imx-image-multimedia is building successfully.
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8qmmek source imx-setup-release.sh -b build-xwayland
bitbake imx-image-multimedia
After flashing SD card image, imx8qmmek booted from the SD card.
I checked the Linux version with following command on imx8qmmek .
cat /proc/version
Linux version 5.4.47-lts-lf-5.4.y+g88b2efd (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Mon Apr 5 09:42:03 UTC 2021
Why was an image that was not the intended version built?
Regards
Ryota Fujiwara
Solved! Go to Solution.
Hello NXP TechSupport
>Have you download success the images you build to the SD card? Or the board boot from the default image on SD card?
Yes.I checked linux kernel version after flash image built successful.
And I also confirm version from tmp/work/imx8qmmek-poky-linux/linux-imx/5.4-r0/git/Makefile
Have you download success the images you build to the SD card? Or the board boot from the default image on SD card? Here recommend you try the images you build to download to emmc and then boot up the boot from emmc to if the version is still. Then contact us.
Hello NXP TechSupport
>Have you download success the images you build to the SD card? Or the board boot from the default image on SD card?
Yes.I checked linux kernel version after flash image built successful.
And I also confirm version from tmp/work/imx8qmmek-poky-linux/linux-imx/5.4-r0/git/Makefile
Good news it works, and thanks a lot for sharing. Wish you have a nice day