Hi,
I am using IMX6ULL , I have generated the image in yocto using bitbake fsl-image-gui.
I have successfully flashed the image through SDcard using .sdcard image.
But if we remove the sdcard it wont boot.
So i need to flash board in emmc or Nand flash. I used UUU utility for flashing through serial getting like Bad Linux ARM zImage magic!
=>
Below i have attached the errors while using UUU.
Please try to help me in flashing the board through Emmc or NAND
Hi @igorpadykov thanks for the reply.
Actually i have downloaded UUU version 1.3.102 by using link https://github.com/NXPmicro/mfgtools/releases/tag/uuu_1.3.102
But I untar that and getting error while installing UUU.
I tried cmake .
after that make
Getting the error like below:
root@teju:/home/teju/Downloads/mfgtools-uuu_1.3.102# make
[ 3%] Generating gitversion.h
build not in appveyor
mv: cannot stat '/home/teju/Downloads/mfgtools-uuu_1.3.102/libuuu/gen/gitversion.h.tmp': No such file or directory
libuuu/CMakeFiles/uuc_s.dir/build.make:61: recipe for target 'libuuu/gitversion.h' failed
make[2]: *** [libuuu/gitversion.h] Error 1
CMakeFiles/Makefile2:85: recipe for target 'libuuu/CMakeFiles/uuc_s.dir/all' failed
make[1]: *** [libuuu/CMakeFiles/uuc_s.dir/all] Error 2
Makefile:127: recipe for target 'all' failed
make: *** [all] Error 2
Hi tejush44
are you using uboot/linux from official nxp source.codeaurora.org/external/imx/linux-imx repository
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.24_2.1.0
https://source.codeaurora.org/external/imx/uboot-imx/tree/?h=imx_v2020.04_5.4.24_2.1.0
Best regards
igor
Hi @igorpadykov
I built images using yocto by using NXP official repo
Hi Teju
for L4.1.15 nxp supported mfg tools as described in Documentation
suggest to use releases which support uuu tool, description can be found
in linux documentation (Release Notes) on
Best regards
igor
Hi @igorpadykov
Thanks for the reply,
I have downloaded the mfgtool as per that document L4.1.15_2.0.0-ga_mfg-tools.
I have downloaded that in ubuntu, Can u please explain me how to use that i am new to this tool.
Actually i have booted board by SDcard. Please suggest me to boot image in nand or emmc flash.
Thanks
Teju S H
Hi Teju
one can look at
https://community.nxp.com/t5/FTF-2015-Training-Presentations/AMF-ACC-T1652/ta-p/1119908
Best regards
igor
Hi Teju
yes the same things can be done with uuu, it is supported in latest linux releases
described on
Best regards
igor
Hi tejush44
reason may be wrong uuu/uboot/bsp versions, as they should be aligned as
described in Release Notes of each BSP available on
https://github.com/NXPmicro/mfgtools/releases
Best regards
igor