Flashing NAND using JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing NAND using JTAG

2,866 Views
gatelogic
Contributor I

Hi,

I have a custom i.MX28 board without SD / USB client, and want to flash the NAND via JTAG.  I'm currently using OpenOCD with the Olimex ARM-USB-OCD JTAG interface.

It appears that there's no current support in OpenOCD for the GPMI-based NAND access used on the i.MX28, which leads me to ask if anyone has used other tools to do the job, or indeed modified OpenOCD to handle it?

Labels (1)
0 Kudos
Reply
2 Replies

2,145 Views
janryll
Contributor I

Hi Alister,

did you get any response to your question?

I have the same question and did not find any answer.

best regards

Jan

0 Kudos
Reply

2,145 Views
sinanakman
Senior Contributor III

Alister, Jan

If you are using OpenOCD, once you halt the SoC soon after

reset, you might be able to load ram version of u-boot and

provided that your NAND flash is supported in u-boot, you

would be able to program your NAND. I didn't try this but I

believe it would work.

Hope this helps

Sinan Akman

0 Kudos
Reply