FlashLoader tool for imxRT1172

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlashLoader tool for imxRT1172

2,365 Views
Shiva-2022
Contributor III

Hello Support Team,

We are working on i.MX RT 1172 microcontroller.

We wanted to test the booting from NAND flash to RAM.

Do we have any FLashloader tool for flashing the bootloable image to External flash i.e., NAND Flash.

 

We have checked in the NXP the forum topics related to Flashloader ( found flash loader for i.MX-RT1050), but we didn't find any flashloader for flashing the External NAND flash (custom board ) for i.MX RT 1172 board.

 

Please suggest.

Thank you.

 

 

0 Kudos
Reply
3 Replies

2,358 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Flashloader for RT1170 is located in the MCU boot middleware from the SDK. You can use MCUBootUtility or Secure Provisioning Tool to load an image on your custom device.
MCUBootUtility:
GitHub - JayHeng/NXP-MCUBootUtility: A one-stop boot utility tool based on Python2.7+wxPython4.0, it...

SPT: MCUXpresso Secure Provisioning Tool | NXP Semiconductors

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply

2,352 Views
Shiva-2022
Contributor III

Hello Omar_Anguiano,

Thanks for the inputs.
We are looking for flashloader for I.MXRT1172.
Can i use RT1170 flashloader for RT1172 ?
if yes, please mention changes required for the same.

Please suggest.
Thank you.

0 Kudos
Reply

2,345 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, the RT1170 Flashloader is compatible with the RT117x family. 

Best regards,
Omar

0 Kudos
Reply