FlashLoader tool for imxRT1172

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlashLoader tool for imxRT1172

2,380件の閲覧回数
Shiva-2022
Contributor III

Hello Support Team,

We are working on i.MX RT 1172 microcontroller.

We wanted to test the booting from NAND flash to RAM.

Do we have any FLashloader tool for flashing the bootloable image to External flash i.e., NAND Flash.

 

We have checked in the NXP the forum topics related to Flashloader ( found flash loader for i.MX-RT1050), but we didn't find any flashloader for flashing the External NAND flash (custom board ) for i.MX RT 1172 board.

 

Please suggest.

Thank you.

 

 

0 件の賞賛
返信
3 返答(返信)

2,373件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Flashloader for RT1170 is located in the MCU boot middleware from the SDK. You can use MCUBootUtility or Secure Provisioning Tool to load an image on your custom device.
MCUBootUtility:
GitHub - JayHeng/NXP-MCUBootUtility: A one-stop boot utility tool based on Python2.7+wxPython4.0, it...

SPT: MCUXpresso Secure Provisioning Tool | NXP Semiconductors

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信

2,367件の閲覧回数
Shiva-2022
Contributor III

Hello Omar_Anguiano,

Thanks for the inputs.
We are looking for flashloader for I.MXRT1172.
Can i use RT1170 flashloader for RT1172 ?
if yes, please mention changes required for the same.

Please suggest.
Thank you.

0 件の賞賛
返信

2,360件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, the RT1170 Flashloader is compatible with the RT117x family. 

Best regards,
Omar

0 件の賞賛
返信