Flash stuck in "No device connected" when using mfgtool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash stuck in "No device connected" when using mfgtool

1,208 次查看
MadPony
Contributor I

I have an i.MX 6ULL EVK and I want to flash the uboot, kernel... using mfgtool. I insert my empty microSD card and connect the USB OTG port to my computer. SW602 set to serial downloader mode and SW601 set to MicroSD. The mfgtool can recognize the USB port and start to load kernel successfully. But when it shows " jump to OS image" the USB port seems disappear and "No device connected" shows up. When I push the reset button, I get the same failure.

0 项奖励
回复
3 回复数

1,202 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,
 
Please help me providing the following information:
MFGTool version that you are using for flashing
Uboot version
Kernel version
Prebuilt image from NXP webpage or your own built image

Best regards,
Aldo.

0 项奖励
回复

1,200 次查看
MadPony
Contributor I

Mfgtool version is L4.9.88_2.0.0_mfg-tool

I did not add my uboot or kernel image to the file. I just clicked mfgtool2-yocto-mx-evk-sdcard-sd2.vbs and I guess it would flash the default images which already exist in the file, correct?

0 项奖励
回复

1,181 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Yes, that is correct it should work that way, are you running the MFGTool in a windows 10 PC?
If yes is there any possibility to try on a windows 7 PC on your side?

Best regards,
Aldo.

0 项奖励
回复