Flash mimxrt1010 on Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash mimxrt1010 on Linux

891件の閲覧回数
MKlem
Contributor III

Hi all,

 

I have got quite a few hours in this problem but still can't get it solved. 

This is the situation. A custom IMX RT1010 board will be put into a fixture where probes are connecting to the SWD port (and others). 

The SWD port is then connected to a MCULink probe, which is connected to an Odroid (ARM64) as the "host". 

The host runs teststeps and one of the first step is to write a program to the board's flash. This is what I already tried:

- Sysprogs openOCD with (custom) flashloader, however the openOCD version of sysprogs is not made for Linux (issue #14)

- Linkserver, but there is no ARM64 version (already had contact with NXP expert)

- pyocd with evkmimxrt1010_flashloader binary as flashloader, but when reporting the flash it does not recognize imxrt flash driver. 

Long story short I am running out of ideas on how to program my flash through the SWD port of the IMXRT1010. It shouldn't be so hard to do right? 

I mean, MCUXpresso also uses a flashdriver, MIMXRT1010_SFDP_QSPI.cfx (elf) but this also does not seem to work. 

With OpenOCD I did manage to get a connection to the CPU and I am also able to halt, run reset etc. Even setting the QE bit in the flash is done. But without a proper flashloader, the same error remains: error writing at address 0x60000000. 

So here I am reaching out, hoping somebody else can give some more pointers where to search, maybe some help on a flashdriver solution... 

Any help is highly appreciated!

 

Thanks,

 

Marcel

0 件の賞賛
返信
1 返信

843件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @MKlem ,

 

The MCUXpresso IDE has Linux version for 64bit, did you try this before? 

Kan_Li_0-1743651171845.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信