Flash loader script file (.DS) for debugging QSPI2 using DS-5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash loader script file (.DS) for debugging QSPI2 using DS-5

1,560件の閲覧回数
ozu
Contributor III

Can anyone share a sample flash loader script file with .DS extension?

I want to debug my image which I have kept in QSPI2 using DS-5.

I have the configuration file (from the QSPI manufacturer) for QSPI but what I am looking for is a script which will enable DS-5 to debug the image.

Thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

1,487件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ozu

please look at arm community how to use DS-5 with i.MX6SX

Software Development Tools: Using DS-5 with the... | ARM Connected Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信