Flash loader script file (.DS) for debugging QSPI2 using DS-5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash loader script file (.DS) for debugging QSPI2 using DS-5

1,571 Views
ozu
Contributor III

Can anyone share a sample flash loader script file with .DS extension?

I want to debug my image which I have kept in QSPI2 using DS-5.

I have the configuration file (from the QSPI manufacturer) for QSPI but what I am looking for is a script which will enable DS-5 to debug the image.

Thanks!

Labels (2)
0 Kudos
Reply
1 Reply

1,498 Views
igorpadykov
NXP Employee
NXP Employee

Hi ozu

please look at arm community how to use DS-5 with i.MX6SX

Software Development Tools: Using DS-5 with the... | ARM Connected Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply