Fix_eboot.exe requires debug DLLs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fix_eboot.exe requires debug DLLs

1,115件の閲覧回数
dougschwanke
Contributor IV

We tried to create a CE image on an SD card using a non-development machine.  When we run Fix_eboot.exe, we get the error message:

"This application has failed to start because the application configuration is incorrect.  Reinstalling the application may fix this problem."

When I reviewed the error in Event Viewer, I saw that the error is due to missing VC90/DebugCRT.  I thought that I only had to install Microsoft Visual C++ 2008 Redistributable Package and 2008 SP1, as there isn't a 2009 Redistributable Package.  Then I realized that it is asking for a "DEBUG" DLL.  This is not provided in MSFT distribution packages. 

Can you provide us with an executable build in release mode?

BTW: MfgTool.exe works just fine.


ラベル(1)
0 件の賞賛
返信
0 返答(返信)