Firmware Configuration Block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Configuration Block

Jump to solution
1,880 Views
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of sect 8.5.2.3 Firmware Configuration Block description of Firmware1_startingPage has only 4Byte.

Here can be specified, Is Block and Page of address?

Is it  page address only specified?. (In the same block, put the Firmware?)

Labels (2)
0 Kudos
Reply
1 Solution
1,766 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

Firmware1_startingPage is absolute page address,

that is Block= Firmware1_startingPage/Number Pages in Block


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


View solution in original post

0 Kudos
Reply
1 Reply
1,767 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

Firmware1_startingPage is absolute page address,

that is Block= Firmware1_startingPage/Number Pages in Block


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 Kudos
Reply