Firmware Configuration Block

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware Configuration Block

ソリューションへジャンプ
1,918件の閲覧回数
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of sect 8.5.2.3 Firmware Configuration Block description of Firmware1_startingPage has only 4Byte.

Here can be specified, Is Block and Page of address?

Is it  page address only specified?. (In the same block, put the Firmware?)

ラベル(2)
0 件の賞賛
返信
1 解決策
1,804件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

Firmware1_startingPage is absolute page address,

that is Block= Firmware1_startingPage/Number Pages in Block


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,805件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

Firmware1_startingPage is absolute page address,

that is Block= Firmware1_startingPage/Number Pages in Block


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 件の賞賛
返信