File transfer between imx28 and host PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

File transfer between imx28 and host PC

2,469件の閲覧回数
alexaldridge
Contributor I

Hello mates!

I'm quite noob with the imx28 evaluation board. I've been able to flash a kernel to a SD card and boot from there. Also I've been able to log to the board using RS232 terminal.

I'd like to install java and transfer some files from my host PC to the board. Any help would be appreciated.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,357件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use use z-modem protocol in the terminal you are using to connect the board.

First you need to connect the board and run "rz" utility. It will wait for the file to be sent.

Then you need to transfer the file from the terminal.

For example in minicom you need to press Ctrl+A and Z and then S for this option.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,357件の閲覧回数
alexaldridge
Contributor I

Thanks for the suggestion. If I do rz in my mx28 I get: "rz not found".

:smileysad:

0 件の賞賛
返信

2,357件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

You may try using WinSCP on Windows host.

Regards,

Yuri.

0 件の賞賛
返信