File system mounting from eMMC device is time consuming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

File system mounting from eMMC device is time consuming

1,780件の閲覧回数
kiruthikavarada
Contributor III

In IMX6 solo hardware file system mounting consumes lot of time from eMMC device. Logs are

  0.103775] calling  mmc_init+0x0/0x90 @ 1

[    0.103911] initcall mmc_init+0x0/0x90 returned 0 after 0 usecs

[    0.238192] calling  mmc_blk_init+0x0/0x88 @ 1

[    0.238258] initcall mmc_blk_init+0x0/0x88 returned 0 after 51 usecs

[    1.775900] mmc0: no vqmmc regulator found

[    1.780009] mmc0: no vmmc regulator found

[    1.822178] mmc0: SDHCI controller on 2198000.usdhc

[2198000.usdhc] using ADMA

[    1.928100] mmc0: BKOPS_EN bit is not set

t [    1.939648] mmc0: new high speed MMC card at address 0001

[    1.945642] mmcblk0: mmc0:0001 MMC08G 7.32 GiB

[    1.950336] mmcblk0boot0: mmc0:0001 MMC08G partition 1 2.00 MiB

[    1.956490] mmcblk0boot1: mmc0:0001 MMC08G partition 2 2.00 MiB

[    1.962665] mmcblk0rpmb: mmc0:0001 MMC08G partition 3 128 KiB

[    1.977587]  mmcblk0: p1 p2

[    1.997640]  mmcblk0boot1: unknown partition table

[    2.018486]  mmcblk0boot0: unknown partition table

[    4.003353] EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended

[    4.015799] EXT3-fs (mmcblk0p2): [bs=4096, gc=59, bpg=32768, ipg=8112, mo=30c18]

[    4.023220] EXT3-fs (mmcblk0p2): using internal journal

[    4.031589] EXT3-fs (mmcblk0p2): recovery complete

[    4.036402] EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode.

I noticed that the device is detected as high speed device. Is there any way to reduce the file system mounting time from eMMC device.

0 件の賞賛
返信
1 返信

1,381件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

according to the log, your filesystem maybe corrupted so need to spend longer time to recover and mount it.

0 件の賞賛
返信