File list cannot update immediately

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

File list cannot update immediately

2,111 Views
joylin
Contributor II

Hi all,
I got a problem the file manager do not have remove file when the USB storage unmount.


When USB connected, ES File Explorer shows the USB device files under the path /mnt/media_rw/udisk on the imx6-sabresd demo image of android_L5.1.1_2.1.0-ga and then the USB removed the files still listed under /mnt/media_rw/udisk. I need press the refresh button of ES File Explorer to remove the USB device files. Android 5.0.0 Lollipop is also can not auto refresh file list when USB device removed. On the demo image android4.2.2 the file list or removed immediately at /mnt/media_rw/udisk when usb connect or remove. Other mobile phone can auto refresh USB device file instantly on android 5.0.0.

any suggestions are very welcome!

Thnaks!

Joy

Labels (3)
0 Kudos
Reply
2 Replies

1,979 Views
b36401
NXP Employee
NXP Employee

Please try to use some another version of File Explorer. Possibly it helps.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,979 Views
joylin
Contributor II

ES-file-explorer_v4.1.4 the lastest version cannot auto refresh file list when USB mount/umount on android 5.0 Lollipop but other android5.0 mobile phone can refresh.
android_L5.0 cannot auto refresh file list with es-file-explorer_v3.0.5.3 but android4.2.2 can.
android_L5.0 cannot auto refresh file list with es-file-explorer_v4.1.4 but android4.2.2 can.
android_L5.1 cannot auto refresh file list with es-file-explorer_v4.1.4.

any idea for refresh implementation.

Thanks!

 

Joy

0 Kudos
Reply