Fetcher failure for URL: 'git://git.alsa-project.org/tinycompress.git;protocol=git;branch=master'. U

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fetcher failure for URL: 'git://git.alsa-project.org/tinycompress.git;protocol=git;branch=master'. U

5,904 Views
pengluo
Contributor III

openil 2.0

bitbake -k nxp-image-real-time-edge

 

Fetcher failure for URL,how to do ?   who can help me ?  see log.rar

 

ERROR: tinycompress-1.1.6-r0 do_fetch: Fetcher failure for URL: 'git://git.alsa-bitbake -k nxp-image-real-time-edgeproject.org/tinycompress.git;protocol=git;branch=master'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/nie/yocto-real-time-edge/buildix8mmevk-bm/tmp/work/cortexa53-crypto-poky-linux/tinycompress/1.1.6-r0/temp/log.do_fetch.20625
ERROR: Task (/home/nie/yocto-real-time-edge/sources/meta-imx/meta-sdk/recipes-multimedia/tinycompress/tinycompress_1.1.6.bb:do_fetch) failed with exit code '1'

0 Kudos
Reply
6 Replies

5,201 Views
Esramirez
Contributor I

I am facing similar issue with the kirkstone distribution.

Does anyone know how to fix This issue?

0 Kudos
Reply

5,870 Views
pengluo
Contributor III

I have solve this question ,thanks

0 Kudos
Reply

5,396 Views
Kusuma
Contributor II

Hi i have also facing same issues , can i know how did u solved.

thanks

0 Kudos
Reply

5,887 Views
jimmychan
NXP TechSupport
NXP TechSupport

which version of BSP are you using?

which package/image do you want to build?

0 Kudos
Reply

5,385 Views
Kusuma
Contributor II


I have solve this question ,thanks
thanks NXP
0 Kudos
Reply

5,258 Views
mallibeerala
Contributor III

I am also facing same Issue, Please help us to resolve this Issue.

Thanks,
Mallikarjuna B.

0 Kudos
Reply