Features of 4th Gen EPD Controller in i.MX7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Features of 4th Gen EPD Controller in i.MX7?

1,093 Views
teazia
Contributor I

I would like to know the features of the 4th Generation EPD controller in the i.MX7 as opposed to earlier generations.  Is this generation of features also avialble in a discrete Controller that is not an embedded on a SOC?

Thank you!

Labels (2)
0 Kudos
Reply
1 Reply

983 Views
art
NXP Employee
NXP Employee

For the detailed description of the i.MX7Dual EPD Controller feature set, please refer to the Section 13.6 of the i.MX7Dual Reference Manual document, available on the processor's Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

NXP does not provide a discrete EPD Controller solution.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply