Fastet way for UART recv handling i.MX6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fastet way for UART recv handling i.MX6ull

681 Views
imx6ull_user_91522
Contributor I

Hello community,

I am using an i.mx6ull with Linux for reading data over UART5 (/dev/ttymxc4).
I need to set a system timestamp for incoming data that should be of precision < 1ms. 

What is the best way to read from UART and get fastest handling of incoming data to set most accurate timestamp?

So far I have done:
Linux Kernel is 5.10.76 with the PREEMPT_RT patch applied.
Set priority of kernel task 'irq/21f4000' to 98 for fast interrupt handling.
I set CPUIDLE states1 and state2 to disabled for fast wakeup.
CPU scaling govenor is set to userspace with max frequency 792 MHz.
I did setserial /dev/ttymxc4 low_latency

I have an user space task that runs at priority 98 for reading the data.
Basically all works fine and I get an accuracy of 50 µs standard deviation. But sometimes also slightly over 1 ms. I want to improve this to get below 1 ms.



Pseudo code of the reading task:

ttymxc4_fd = ::open("/dev/ttymxc4", O_RDWR | O_NOCTTY | O_NDELAY);
struct pollfd = pollSrc;

pollSrc.fd = ttymxc4_fd;
pollSrc.events = POLLIN;
pollfd.revents = 0;
...
while(true)
{
poll(&pollSrc, 1)
clock_gettime(CLOCK_REALTIME, &recvTimestamp);
read(ttymxc4_fd, read_buf, sizeof(read_buf));
...
}

Any advice for improving that? Thank you in advance.

 

Labels (2)
0 Kudos
Reply
1 Reply

589 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

It seems that you have done it quite well, aside from what you have arleady done I think that I would be possible to achieve below 1mS, for this it may be needed to hack a bit the process.

Like creating a task that have priority and mute all other proces so it handle the interrupt for the timestamp on time, but this could cause some issues on the other proces that may be running on your system.

Best regards/Saludos,
Aldo.

0 Kudos
Reply