Fastboot issue for IMX6Q Android Kitkat 4.4 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fastboot issue for IMX6Q Android Kitkat 4.4 BSP

4,320件の閲覧回数
changyuheng
Contributor II

I tried update image by fastboot on IMX6 custom board (refer to sabresd board), but something was wrong at first step,

I can't connect to device and error message as following:

MX6Q SABRESD U-Boot > fastboot                                            
fastboot is in init......flash target is MMC:2                            

wait usb cable into the connector!

Correct me if I'm wrong,

I think the pin definition should be modified,

but I don't know which pin?

Thank you!

ラベル(3)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,650件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Public Account

had you attached USB cable between host PC and i.MX6 USB OTG,

as describes attached document sect.8.2 How do I use Android fastboot?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,650件の閲覧回数
changyuheng
Contributor II

I know~ but it works on kernel for adb mode, why u-boot fastboot mode failed?

it's no problem for pin difinition, have any ways to solve this issue?

thanks

0 件の賞賛
返信

3,650件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

seems Uboot does not support USB.

USB is supported only in latest Uboot releases:

version v2014.04 (L3.10.53 kernel).

~igor