Fast Boot achieved is possible with NAND flash or XIP NOR Flash??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fast Boot achieved is possible with NAND flash or XIP NOR Flash??

1,270 次查看
sagar_kumar
Contributor I

Hi

 

We need fast boot in my i.MX6 Quad based medical tablet application. Can you tell me if 256MB NOR FLASH (MT25QL02GCBB8E12-0SIT) in QSPI mode is suitable for fast boot? or we have to use NAND flash to achieve Fast Boot in my application?

 

 

 

Thanks

Sagar

标签 (1)
0 项奖励
回复
1 回复

1,212 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

i.MX6Q does not support qspi boot, for fast boot one can check overview on

Android Fastboot implementation for i.MX 

Booting i.MX6 under one second - i.MXDev Blog 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复