Fast Boot achieved is possible with NAND flash or XIP NOR Flash??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fast Boot achieved is possible with NAND flash or XIP NOR Flash??

1,273 Views
sagar_kumar
Contributor I

Hi

 

We need fast boot in my i.MX6 Quad based medical tablet application. Can you tell me if 256MB NOR FLASH (MT25QL02GCBB8E12-0SIT) in QSPI mode is suitable for fast boot? or we have to use NAND flash to achieve Fast Boot in my application?

 

 

 

Thanks

Sagar

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

i.MX6Q does not support qspi boot, for fast boot one can check overview on

Android Fastboot implementation for i.MX 

Booting i.MX6 under one second - i.MXDev Blog 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply