I have a 4.19 linux ubuntu distro running on my LS1021-TWR evaluation kit and I am trying to make the dbus works on the device.
I really do not think this is dependent on what boards I am using
However, I have encountered the following error which I could not figure out:
Failed to open connection to "session" message bus: Unable to autolaunch a dbus-daemon without a $DISPLAY for X11
I found something that says about this issue but I still do not have any clues about the cause.
https://bugs.debian.org/cgi-bin/bugreport.cgi?bug=690530
Hope someone can help.
解決済! 解決策の投稿を見る。
Such error message means that you need to assign a display to the application.
I mean you need to perform something like "export DISPLAY=:0" prior to running it.
Such error message means that you need to assign a display to the application.
I mean you need to perform something like "export DISPLAY=:0" prior to running it.
I fixed it by performed the following commands on the command line:
(1)DISPLAY=":0" DBUS_SESSION_BUS_ADDRESS="unix:path=/run/dbus/system_bus_socket"
(2)export DBUS_SESSION_BUS_ADDRESS
but later on:
when I ran dbus on this device I always encountered this error below: any one knows why?
$2 = (gchar *) 0xb2c05668 "GDBus.Error:org.freedesktop.DBus.Error.ServiceUnknown: The name org.byos.server was not provided by any .service files"
this is the debug statement from the gdb