Hi,
I'm trying to port Android L5.0.0-1.0.0 on our custom board, but fail to boot into system image.
From the boot log, looks like VERITY_METADATA_MAGIC_NUMBER can't be read and fail to mount mmcblk3p5.
fs_mgr: Couldn't find verity metadata at offset 0! fs_mgr: Could not set up verified partition, skipping! EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option EXT4-fs (mmcblk3p4): recovery complete EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0 EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option EXT4-fs (mmcblk3p6): recovery complete EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0 EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null) fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0 |
Could someone give me a hint which step or setting I missed?
What should I do to keep verified boot enabled and mount system image successfully, except "androidboot.dm_verity=disabled"?
Thanks,
Oliver
Original Attachment has been moved to: boot_failed.log.zip
How do you get the boot log? I might have the same problem, but I don't know how to see that! When you run the MfgTool, it looks like it formats everything, so I can't reboot with a valid system.img to use the device. When it doesn't boot, how do you interact with the board to read something from it?