Failed to mount system image!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to mount system image!

2,127 Views
oliverkuo
Contributor IV

Hi,

 

  I'm trying to port Android L5.0.0-1.0.0 on our custom board, but fail to boot into system image.

From the boot log, looks like VERITY_METADATA_MAGIC_NUMBER can't be read and fail to mount mmcblk3p5.

fs_mgr: Couldn't find verity metadata at offset 0!

fs_mgr: Could not set up verified partition, skipping!

EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p4): recovery complete

EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p6): recovery complete

EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0

Could someone give me a hint which step or setting I missed?

What should I do to keep verified boot enabled and mount system image successfully, except "androidboot.dm_verity=disabled"?

 

Thanks,

Oliver

Original Attachment has been moved to: boot_failed.log.zip

Labels (3)
0 Kudos
Reply
2 Replies

994 Views
jonathantaylor
Contributor II

How do you get the boot log?  I might have the same problem, but I don't know how to see that!  When you run the MfgTool, it looks like it formats everything, so I can't reboot with a valid system.img to use the device.  When it doesn't boot, how do you interact with the board to read something from it?

0 Kudos
Reply

994 Views
oliverkuo
Contributor IV

Hi,

You could download your image by modifying the script of MFGTool.

Please refer to the document of MFGTool for detail.

Best regards,

Oliver

0 Kudos
Reply