Failed to fetch URL git://github.com/nxp-imx/linux-imx.git

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to fetch URL git://github.com/nxp-imx/linux-imx.git

5,830件の閲覧回数
khang_letruong
Senior Contributor III

Hi Community,

I am not sure if it was an issue of the network but I am struggling with the bitbaking of an imx-image of Yocto LF6.6.3-1.0.0 during the fetching of linux-imx :

Initialising tasks: 100% |############################################################| Time: 0:00:00
Sstate summary: Wanted 1 Local 0 Mirrors 0 Missed 1 Current 163 (0% match, 99% complete)
NOTE: Executing Tasks
WARNING: linux-imx-6.6.3+git-r0 do_fetch: Failed to fetch URL git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-6.6.y, attempting MIRRORS if available
ERROR: linux-imx-6.6.3+git-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export PATH="/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/sysroots-uninative/x86_64-linux/usr/bin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/sources/poky/scripts:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot/usr/bin/crossscripts:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot-native/usr/sbin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot-native/usr/bin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot-native/sbin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/recipe-sysroot-native/bin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/sources/poky/bitbake/bin:/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/hosttools"; export HOME="/home/dynim"; LANG=C git -c gc.autoDetach=false -c core.pager=cat clone --bare --mirror https://github.com/nxp-imx/linux-imx.git /home/dynim/yocto_dl/v6.6//git2/github.com.nxp-imx.linux-imx.git --progress failed with exit code 128, no output
ERROR: linux-imx-6.6.3+git-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-6.6.y')
ERROR: Logfile of failure stored in: /workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/build-xwayland.evk/tmp/work/imx8mpevk-poky-linux/linux-imx/6.6.3+git/temp/log.do_fetch.19916
ERROR: Task (/workdir/polyhex-debix_model_a-yocto-bsp-6_6_3-1_0_0/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 538 tasks of which 537 didn't need to be rerun and 1 failed.

 

I am using docker Ubuntu-22.04 as compilation environment.

Best Regards,
Khang

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

5,788件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @khang_letruong!

Thank you for contacting NXP Support!

 

I can't reproduce the error.

Chavira_0-1722262388019.pngChavira_0-1722262388019.png

 

Maybe the error is caused by your environment.

 

I am using Ubuntu 22.04 too.

 

Best Regards!

Chavira

 

0 件の賞賛
返信

5,785件の閲覧回数
khang_letruong
Senior Contributor III

Hi @Chavira,

I was able to clone then compile the linux-imx repo once during the weekend without changing anything in the environment.

Regards,

Khang

5,385件の閲覧回数
GregDyess
Contributor III

I am having the exact same problem.  I have tried on multiple systems with the same result.

 

0 件の賞賛
返信