Failed to fetch URL crate://crates.io/parsec-service/1.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Failed to fetch URL crate://crates.io/parsec-service/1.2.0

跳至解决方案
2,128 次查看
gufengzi
Contributor III

how to understand  crate://crates.io/parsec-service/1.2.0?

it is not a website.

jt@kylin:~/src/yocto_imx/build-qpxwayland$ bitbake -c fetch parsec-service
Loading cache: 100% |#############################################################################################################################################| Time: 0:00:01
Loaded 5303 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.4.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qpsabresd"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.1-mickledore"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:0a98281d37b0bd8dc1548c390216cb3978e36e0e"
meta-oe
meta-multimedia
meta-python = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842"
meta-freescale = "HEAD:9b00d40b787c2b7105ce209f5635cc1a0cab81ca"
meta-freescale-3rdparty = "HEAD:93ba05e3a16a028b770fa1e813b13eb87a59ac63"
meta-freescale-distro = "HEAD:b09c18a3f649f0cf1b40432bb39e76ba16fe94e2"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:6efe87f014c5bdcbda30f06156ee11d8bc3dc7fe"
meta-nxp-demo-experience = "HEAD:7f34a32c7877e55e87b6a99e90da4128ed632bf2"
meta-arm
meta-arm-toolchain = "HEAD:0e043288fd0b17fbf31cf00ae33045107a991144"
meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang = "HEAD:af4dcba009ba98250315520f3003fde4ee164cce"
meta-gnome
meta-networking
meta-filesystems = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842"
meta-qt6 = "HEAD:1406d0a85525a71fe5d7892d7f915404290a78ad"
meta-parsec
meta-tpm = "HEAD:d7db0a3bd1a8639df7570483f003ce00cbe274a2"
meta-virtualization = "HEAD:56593e277a377157944a6676e57497066b770a35"

Initialising tasks: 100% |################################################################################################################################| Time: 0:00:00
Sstate summary: Wanted 0 Local 0 Mirrors 0 Missed 0 Current 0 (0% match, 0% complete)
NOTE: No setscene tasks
NOTE: Executing Tasks
WARNING: parsec-service-1.2.0-r0 do_fetch: Failed to fetch URL crate://crates.io/parsec-service/1.2.0, attempting MIRRORS if available
ERROR: parsec-service-1.2.0-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus,guid=c45449a1743232ee952938956594d275"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/tjt/src/yocto_imx/build-qpxwayland/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/usr/bin/python3-native:/home/tjt/src/yocto_imx/sources/poky/scripts:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot/usr/bin/crossscripts:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/usr/sbin:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/usr/bin:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/sbin:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/recipe-sysroot-native/bin:/home/tjt/src/yocto_imx/sources/poky/bitbake/bin:/home/tjt/src/yocto_imx/build-qpxwayland/tmp/hosttools"; export HOME="/home/tjt"; /usr/bin/env wget -t 2 -T 30 --passive-ftp -O /home/tjt/src/yocto_imx/downloads/parsec-service-1.2.0.crate.tmp -P /home/tjt/src/yocto_imx/downloads/ 'https://crates.io/api/v1/crates/parsec-service/1.2.0/download' --progress=dot -v failed with exit code 5, no output
ERROR: parsec-service-1.2.0-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'crate://crates.io/parsec-service/1.2.0')
ERROR: Logfile of failure stored in: /home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/parsec-service/1.2.0-r0/temp/log.do_fetch.834532
ERROR: Task (/home/tjt/src/yocto_imx/sources/meta-security/meta-parsec/recipes-parsec/parsec-service/parsec-service_1.2.0.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/tjt/src/yocto_imx/sources/meta-security/meta-parsec/recipes-parsec/parsec-service/parsec-service_1.2.0.bb:do_fetch
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.
tjt@kylin:~/src/yocto_imx/build-qpxwayland$

0 项奖励
回复
1 解答
2,112 次查看
Harvey021
NXP TechSupport
NXP TechSupport

how to understand crate://crates.io/parsec-service/1.2.0?

-> Crate Fetcher (crate://)

This submodule fetches code for Rust language “crates” corresponding to Rust libraries and programs to compile. Such crates are typically shared on https://crates.io/ but this fetcher supports other crate registries too.

The format for the SRC_URI setting must be:

SRC_URI = "crate://REGISTRY/NAME/VERSION"

Here is an example URL:

SRC_URI = "crate://crates.io/glob/0.2.11"

 

Regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,113 次查看
Harvey021
NXP TechSupport
NXP TechSupport

how to understand crate://crates.io/parsec-service/1.2.0?

-> Crate Fetcher (crate://)

This submodule fetches code for Rust language “crates” corresponding to Rust libraries and programs to compile. Such crates are typically shared on https://crates.io/ but this fetcher supports other crate registries too.

The format for the SRC_URI setting must be:

SRC_URI = "crate://REGISTRY/NAME/VERSION"

Here is an example URL:

SRC_URI = "crate://crates.io/glob/0.2.11"

 

Regards

Harvey

0 项奖励
回复