Failed to capture correct image from OV10633 on MX6Q CSI0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to capture correct image from OV10633 on MX6Q CSI0

2,081 Views
RobbieJiang
Contributor IV

Hi all,

We are working on supporting OV10633 on MX6Q/Linux platform.

OV10633 is connected to SOC through CSI0 port.

By now, we can capture image from CSI0, but the image is corrupted (as the attachment).

Seems that there is something wrong with synchronization.

However, I'm not sure if there is anything wrong with the MX6Q CSI configuration.

OV10633 input clock (XVCLK) is 24MHz, and it outputs PIXCLK/VSYNC/HREF signals

and 8-bit UYVY parallel data.  And these output signals look good.

On the other side,  MX6Q CSI0 is configured in gated-mode, 8-bit data width, UYVY format, 

and the data destination is IDMAC via SMFC. ( IPU0_CSI0_SENS_CONF is 0x04008A00 )

Following is the IPU and CSI configuration:

imx-ipuv3 imx-ipuv3.0: init channel = 15

imx-ipuv3 imx-ipuv3.0: initializing idma ch 0 @ c08c0000

imx-ipuv3 imx-ipuv3.0: ch 0 word 0 - 00000000 00000000 00000000 E0001800 000B3C9F

imx-ipuv3 imx-ipuv3.0: ch 0 word 1 - 03240000 00648000 0147C000 00027FC0 00000000

imx-ipuv3 imx-ipuv3.0: PFS 0xa,

imx-ipuv3 imx-ipuv3.0: BPP 0x3,

imx-ipuv3 imx-ipuv3.0: NPB 0x1f

imx-ipuv3 imx-ipuv3.0: FW 1279,

imx-ipuv3 imx-ipuv3.0: FH 719,

imx-ipuv3 imx-ipuv3.0: EBA0 0x19200000

imx-ipuv3 imx-ipuv3.0: EBA1 0x19200000

imx-ipuv3 imx-ipuv3.0: Stride 2559

imx-ipuv3 imx-ipuv3.0: scan_order 0

imx-ipuv3 imx-ipuv3.0: uv_stride 0

imx-ipuv3 imx-ipuv3.0: u_offset 0x0

imx-ipuv3 imx-ipuv3.0: v_offset 0x0

imx-ipuv3 imx-ipuv3.0: Width0 0+1,

imx-ipuv3 imx-ipuv3.0: Width1 0+1,

imx-ipuv3 imx-ipuv3.0: Width2 0+1,

imx-ipuv3 imx-ipuv3.0: Width3 0+1,

imx-ipuv3 imx-ipuv3.0: Offset0 0,

imx-ipuv3 imx-ipuv3.0: Offset1 0,

imx-ipuv3 imx-ipuv3.0: Offset2 0,

imx-ipuv3 imx-ipuv3.0: Offset3 0

imx-ipuv3 imx-ipuv3.0: IPU_CONF =       0x00000101

imx-ipuv3 imx-ipuv3.0: IDMAC_CONF =     0x0000002F

imx-ipuv3 imx-ipuv3.0: IDMAC_CHA_EN1 =  0x00000001

imx-ipuv3 imx-ipuv3.0: IDMAC_CHA_EN2 =  0x00000000

imx-ipuv3 imx-ipuv3.0: IDMAC_CHA_PRI1 =         0x18800001

imx-ipuv3 imx-ipuv3.0: IDMAC_CHA_PRI2 =         0x00000000

imx-ipuv3 imx-ipuv3.0: IDMAC_BAND_EN1 =         0x00000000

imx-ipuv3 imx-ipuv3.0: IDMAC_BAND_EN2 =         0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_CHA_DB_MODE_SEL0 =   0x00000001

imx-ipuv3 imx-ipuv3.0: IPU_CHA_DB_MODE_SEL1 =   0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_CHA_TRB_MODE_SEL0 =  0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_CHA_TRB_MODE_SEL1 =  0x00000000

imx-ipuv3 imx-ipuv3.0: DMFC_WR_CHAN =   0x00000090

imx-ipuv3 imx-ipuv3.0: DMFC_WR_CHAN_DEF =       0x202020F6

imx-ipuv3 imx-ipuv3.0: DMFC_DP_CHAN =   0x00009694

imx-ipuv3 imx-ipuv3.0: DMFC_DP_CHAN_DEF =       0x2020F6F6

imx-ipuv3 imx-ipuv3.0: DMFC_IC_CTRL =   0x00000002

imx-ipuv3 imx-ipuv3.0: IPU_FS_PROC_FLOW1 =      0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_FS_PROC_FLOW2 =      0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_FS_PROC_FLOW3 =      0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_FS_DISP_FLOW1 =      0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_VDIC_VDI_FSIZE =     0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_VDIC_VDI_C =         0x00000000

imx-ipuv3 imx-ipuv3.0: IPU_IC_CONF =    0x00000000

imx-ipuv3 imx-ipuv3.0: IPU0_CSI0_CONF =         0x04008A00

imx-ipuv3 imx-ipuv3.0: IPU1_CSI1_CONF =         0x00000000

imx-ipuv3 imx-ipuv3.0: IPU0_CSI0_SENS_FRM_SIZE =        0x02CF04FF

imx-ipuv3 imx-ipuv3.0: IPU0_CSI0_ACT_FRM_SIZE =         0x02CF04FF

imx-ipuv3 imx-ipuv3.0: IPU0_CSI0_OUT_FRM_CTRL =         0x00000000

imx-ipuv3 imx-ipuv3.0: IPU1_CSI1_SENS_FRM_SIZE =        0x00000000

imx-ipuv3 imx-ipuv3.0: IPU1_CSI1_ACT_FRM_SIZE =         0x00000000

imx-ipuv3 imx-ipuv3.0: IPU1_CSI1_OUT_FRM_CTRL =         0x00000000

Anything wrong with my IPU/CSI configuration?

Any idea?

Thanks,

Robbie

Labels (3)
0 Kudos
Reply
3 Replies

1,877 Views
jimmychan
NXP TechSupport
NXP TechSupport

can you show the node setting in dtsi file?

0 Kudos
Reply

1,877 Views
RobbieJiang
Contributor IV

jimmy,

Thanks!

We have solved the problem.

Robbie

0 Kudos
Reply

1,877 Views
kiseok_ko
Contributor III

Hi jimmy&Robbie Jiang

I also take problem like yours.

but, It is something different...... our image shows when I short href with ground.( or esd test )

Could you help me how to solve this problem?

best regards & thank you.

kiseokko.

p.s. we use ov10633 & IPU2 CSI1.

0 Kudos
Reply