Failed to boot latest Linux version on IMX8MM-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to boot latest Linux version on IMX8MM-EVK

ソリューションへジャンプ
7,100件の閲覧回数
faraz7321
Contributor I

I have been trying to run latest Linux 5.15.32_2.0.0​ iMX8MMINI but it stops booting and print error in serial output : pcie: PCIe PLL lock timeout and hangs.

The older versions I tried:

  1. Linux 5.10.72_2.2.2
  2. Linux 5.10.72_2.2.0
  3. Linux 5.4.70_2.3.0
  4. Linux 4.14.98_2.0.0 (Worked!)

Please find the attached log file for the reference.

Thank you so much!

 

U-Boot SPL 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC2
NOTICE: BL31: v2.6(release):android-12.0.0_2.0.0-rc1-6-gc6a19b1a3
NOTICE: BL31: Built : 06:37:22, Jun 7 2022


U-Boot 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)

CPU: i.MX8MMQL rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 40C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Power supply on USB1
Core: 168 devices, 30 uclasses, devicetree: separate
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated

BuildInfo:
- ATF c6a19b1

switch to partitions #0, OK
mmc2(part 0) is current device
flash target is MMC:2
Net:
Warning: ethernet@30be0000 (eth0) using random MAC address - a2:2f:c3:b8:c5:ac
eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
starting USB...
Bus usb@32e40000: Port not available.
USB is stopped. Please issue 'usb start' first.
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
Scanning disk [email protected]...
Scanning disk [email protected]...
Found 6 disks
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
48127 bytes read in 4 ms (11.5 MiB/s)
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
switch to partitions #0, OK
mmc2(part 0) is current device
Failed to load 'boot.scr'
30931456 bytes read in 103 ms (286.4 MiB/s)
Booting from mmc ...
48127 bytes read in 11 ms (4.2 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300ebfe
Modify /vpu_g1@38300000:status disabled
Modify /vpu_g2@38310000:status disabled
Modify /vpu_h1@38320000:status disabled
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.15.32-lts-next+gfa6c3168595c (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.38.20220313) #1 SMP PREEMPT Tue Jun 7 02:34:46 UTC 2022
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x95bd1800-0x95bd3fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s41176 r8192 d32552 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 508032
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk2p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1337752K/2064384K available (18560K kernel code, 1534K rwdata, 7072K rodata, 2944K init, 541K bss, 71272K reserved, 655360K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x474/0x660 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000366] Console: colour dummy device 80x25
[ 0.000434] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000448] pid_max: default: 32768 minimum: 301
[ 0.000505] LSM: Security Framework initializing
[ 0.000563] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.000577] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.001832] rcu: Hierarchical SRCU implementation.
[ 0.002766] EFI services will not be available.
[ 0.002941] smp: Bringing up secondary CPUs ...
[ 0.003334] Detected VIPT I-cache on CPU1
[ 0.003361] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.003408] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.003844] Detected VIPT I-cache on CPU2
[ 0.003865] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.003890] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.004332] Detected VIPT I-cache on CPU3
[ 0.004349] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.004372] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.004426] smp: Brought up 1 node, 4 CPUs
[ 0.004442] SMP: Total of 4 processors activated.
[ 0.004448] CPU features: detected: 32-bit EL0 Support
[ 0.004453] CPU features: detected: 32-bit EL1 Support
[ 0.004459] CPU features: detected: CRC32 instructions
[ 0.012241] CPU: All CPU(s) started at EL2
[ 0.012269] alternatives: patching kernel code
[ 0.013676] devtmpfs: initialized
[ 0.019884] KASLR disabled due to lack of seed
[ 0.020066] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.020086] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.043067] pinctrl core: initialized pinctrl subsystem
[ 0.043618] DMI not present or invalid.
[ 0.044040] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.049188] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.049591] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.049948] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.050054] audit: initializing netlink subsys (disabled)
[ 0.050288] audit: type=2000 audit(0.048:1): state=initialized audit_enabled=0 res=1
[ 0.050861] thermal_sys: Registered thermal governor 'step_wise'
[ 0.050867] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.051065] cpuidle: using governor menu
[ 0.051275] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.051372] ASID allocator initialised with 65536 entries
[ 0.052209] Serial: AMBA PL011 UART driver
[ 0.052271] imx mu driver is registered.
[ 0.052292] imx rpmsg driver is registered.
[ 0.063385] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.072937] platform 32e10000.mipi_dsi: Fixing up cyclic dependency with 32e00000.lcdif
[ 0.073598] platform 32e30000.mipi_csi: Fixing up cyclic dependency with 32e20000.csi1_bridge
[ 0.094271] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.094291] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.094299] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.094307] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.095342] cryptd: max_cpu_qlen set to 1000
[ 0.098149] ACPI: Interpreter disabled.
[ 0.098790] iommu: Default domain type: Translated
[ 0.098798] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.098966] vgaarb: loaded
[ 0.099234] SCSI subsystem initialized
[ 0.099538] usbcore: registered new interface driver usbfs
[ 0.099574] usbcore: registered new interface driver hub
[ 0.099600] usbcore: registered new device driver usb
[ 0.100475] mc: Linux media interface: v0.10
[ 0.100501] videodev: Linux video capture interface: v2.00
[ 0.100570] pps_core: LinuxPPS API ver. 1 registered
[ 0.100576] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 0.100595] PTP clock support registered
[ 0.100746] EDAC MC: Ver: 3.0.0
[ 0.101745] FPGA manager framework
[ 0.101821] Advanced Linux Sound Architecture Driver Initialized.
[ 0.102334] Bluetooth: Core ver 2.22
[ 0.102361] NET: Registered PF_BLUETOOTH protocol family
[ 0.102367] Bluetooth: HCI device and connection manager initialized
[ 0.102379] Bluetooth: HCI socket layer initialized
[ 0.102389] Bluetooth: L2CAP socket layer initialized
[ 0.102405] Bluetooth: SCO socket layer initialized
[ 0.103002] clocksource: Switched to clocksource arch_sys_counter
[ 0.103143] VFS: Disk quotas dquot_6.6.0
[ 0.103188] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.103343] pnp: PnP ACPI: disabled
[ 0.109113] NET: Registered PF_INET protocol family
[ 0.109244] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.110182] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.110243] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.110355] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.110588] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.110676] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.110722] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.110849] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.111255] RPC: Registered named UNIX socket transport module.
[ 0.111263] RPC: Registered udp transport module.
[ 0.111270] RPC: Registered tcp transport module.
[ 0.111277] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.111974] PCI: CLS 0 bytes, default 64
[ 0.112506] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.113181] kvm [1]: IPA Size Limit: 40 bits
[ 0.114724] kvm [1]: GICv3: no GICV resource entry
[ 0.114730] kvm [1]: disabling GICv2 emulation
[ 0.114745] kvm [1]: GIC system register CPU interface enabled
[ 0.114822] kvm [1]: vgic interrupt IRQ9
[ 0.114938] kvm [1]: Hyp mode initialized successfully
[ 0.117994] Initialise system trusted keyrings
[ 0.118115] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.124016] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.124603] NFS: Registering the id_resolver key type
[ 0.124631] Key type id_resolver registered
[ 0.124639] Key type id_legacy registered
[ 0.124708] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.124716] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.124739] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.125079] 9p: Installing v9fs 9p2000 file system support
[ 0.161163] Key type asymmetric registered
[ 0.161173] Asymmetric key parser 'x509' registered
[ 0.161230] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.161239] io scheduler mq-deadline registered
[ 0.161247] io scheduler kyber registered
[ 0.167146] EINJ: ACPI disabled.
[ 0.176643] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.176667] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.183092] mxs-dma 33000000.dma-controller: initialized
[ 0.184588] SoC: i.MX8MM revision 1.0
[ 0.185036] Bus freq driver module loaded
[ 0.190481] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.192749] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 47, base_baud = 5000000) is a IMX
[ 0.193284] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 48, base_baud = 5000000) is a IMX
[ 0.193694] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 49, base_baud = 1500000) is a IMX
[ 1.224413] printk: console [ttymxc1] enabled
[ 1.243534] loop: module loaded
[ 1.247963] of_reserved_mem_lookup() returned NULL
[ 1.252844] megasas: 07.717.02.00-rc1
[ 1.258026] imx ahci driver is registered.
[ 1.265625] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[ 1.274521] tun: Universal TUN/TAP device driver, 1.6
[ 1.280427] thunder_xcv, ver 1.0
[ 1.283700] thunder_bgx, ver 1.0
[ 1.286958] nicpf, ver 1.0
[ 1.291666] hclge is initializing
[ 1.295010] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.302240] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.307603] e1000: Intel(R) PRO/1000 Network Driver
[ 1.312495] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.318278] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.323250] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.329221] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.334666] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.340274] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.346550] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.352648] sky2: driver version 1.30
[ 1.356852] usbcore: registered new interface driver r8152
[ 1.362599] VFIO - User Level meta-driver version: 0.3
[ 1.369946] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.376501] ehci-pci: EHCI PCI platform driver
[ 1.380985] ehci-platform: EHCI generic platform driver
[ 1.386400] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.392605] ohci-pci: OHCI PCI platform driver
[ 1.397085] ohci-platform: OHCI generic platform driver
[ 1.403021] usbcore: registered new interface driver uas
[ 1.408376] usbcore: registered new interface driver usb-storage
[ 1.414455] usbcore: registered new interface driver usbserial_generic
[ 1.421006] usbserial: USB Serial support registered for generic
[ 1.427044] usbcore: registered new interface driver ftdi_sio
[ 1.432811] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.440159] usbcore: registered new interface driver usb_serial_simple
[ 1.446708] usbserial: USB Serial support registered for carelink
[ 1.452822] usbserial: USB Serial support registered for zio
[ 1.458502] usbserial: USB Serial support registered for funsoft
[ 1.464532] usbserial: USB Serial support registered for flashloader
[ 1.470905] usbserial: USB Serial support registered for google
[ 1.476844] usbserial: USB Serial support registered for libtransistor
[ 1.483399] usbserial: USB Serial support registered for vivopay
[ 1.489431] usbserial: USB Serial support registered for moto_modem
[ 1.495717] usbserial: USB Serial support registered for motorola_tetra
[ 1.502350] usbserial: USB Serial support registered for novatel_gps
[ 1.508726] usbserial: USB Serial support registered for hp4x
[ 1.514495] usbserial: USB Serial support registered for suunto
[ 1.520436] usbserial: USB Serial support registered for siemens_mpi
[ 1.526824] usbcore: registered new interface driver usb_ehset_test
[ 1.535902] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.550289] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.556507] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.565684] i2c_dev: i2c /dev entries driver
[ 1.570898] mx6s-csi 32e20000.csi1_bridge: initialising
[ 1.579467] Bluetooth: HCI UART driver ver 2.3
[ 1.583934] Bluetooth: HCI UART protocol H4 registered
[ 1.589083] Bluetooth: HCI UART protocol BCSP registered
[ 1.594424] Bluetooth: HCI UART protocol LL registered
[ 1.599570] Bluetooth: HCI UART protocol ATH3K registered
[ 1.604993] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.611350] Bluetooth: HCI UART protocol Broadcom registered
[ 1.617042] Bluetooth: HCI UART protocol QCA registered
[ 1.623832] sdhci: Secure Digital Host Controller Interface driver
[ 1.630032] sdhci: Copyright(c) Pierre Ossman
[ 1.635050] Synopsys Designware Multimedia Card Interface Driver
[ 1.641664] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.649333] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.656494] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.663440] usbcore: registered new interface driver usbhid
[ 1.669024] usbhid: USB HID core driver
[ 1.676852] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.681292] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 1.684976] optee: probing for conduit method.
[ 1.695036] optee: revision 3.17 (c9619a7e)
[ 1.695946] optee: dynamic shared memory is enabled
[ 1.705337] optee: initialized driver
[ 1.710585] galcore: clk_get vg clock failed, disable vg!
[ 1.716329] Galcore version 6.4.3.p4.398061
[ 1.771243] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 1.778353] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0
[ 1.778431] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 1.790697] NET: Registered PF_LLC protocol family
[ 1.792557] mmcblk2: p1 p2
[ 1.796035] NET: Registered PF_INET6 protocol family
[ 1.799551] mmcblk2boot0: mmc2:0001 DG4016 4.00 MiB
[ 1.805309] Segment Routing with IPv6
[ 1.809686] mmcblk2boot1: mmc2:0001 DG4016 4.00 MiB
[ 1.811961] In-situ OAM (IOAM) with IPv6
[ 1.818794] mmcblk2rpmb: mmc2:0001 DG4016 4.00 MiB, chardev (234:0)
[ 1.820893] NET: Registered PF_PACKET protocol family
[ 1.832955] Bluetooth: RFCOMM TTY layer initialized
[ 1.837852] Bluetooth: RFCOMM socket layer initialized
[ 1.843042] Bluetooth: RFCOMM ver 1.11
[ 1.846799] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.852117] Bluetooth: BNEP filters: protocol multicast
[ 1.857356] Bluetooth: BNEP socket layer initialized
[ 1.862326] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.868255] Bluetooth: HIDP socket layer initialized
[ 1.874266] 8021q: 802.1Q VLAN Support v1.8
[ 1.878478] lib80211: common routines for IEEE802.11 drivers
[ 1.884257] 9pnet: Installing 9P2000 support
[ 1.888564] tsn generic netlink module v1 init...
[ 1.893358] Key type dns_resolver registered
[ 1.898526] Loading compiled-in X.509 certificates
[ 1.927171] usb_phy_generic usbphynop1: supply vcc not found, using dummy regulator
[ 1.935101] usb_phy_generic usbphynop2: supply vcc not found, using dummy regulator
[ 1.944672] nxp-pca9450 0-0025: Read device id error
[ 1.949854] i2c i2c-0: IMX I2C adapter registered
[ 1.956010] i2c 1-003d: Fixing up cyclic dependency with 32e10000.mipi_dsi
[ 1.963224] adv7511 1-003d: supply avdd not found, using dummy regulator
[ 1.970032] adv7511 1-003d: supply dvdd not found, using dummy regulator
[ 1.976774] adv7511 1-003d: supply pvdd not found, using dummy regulator
[ 1.983515] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[ 1.990359] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[ 1.997103] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[ 2.004624] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e10000' disabled
[ 2.012444] i2c 1-0050: Fixing up cyclic dependency with 32e40000.usb
[ 2.020808] i2c i2c-1: IMX I2C adapter registered
[ 2.027606] i2c 2-003c: Fixing up cyclic dependency with 32e30000.mipi_csi
[ 2.034916] ov5640_mipi 2-003c: No sensor reset pin available
[ 2.040696] ov5640_mipi 2-003c: supply DOVDD not found, using dummy regulator
[ 2.047942] ov5640_mipi 2-003c: supply DVDD not found, using dummy regulator
[ 2.055035] ov5640_mipi 2-003c: supply AVDD not found, using dummy regulator
[ 2.075308] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 2.080632] ov5640_mipi 2-003c: Camera is not found
[ 2.085803] i2c i2c-2: IMX I2C adapter registered
[ 2.092916] imx6q-pcie 33800000.pcie: supply epdev_on not found, using dummy regulator
[ 2.094947] imx-drm 32c00000.bus:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 2.101179] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.109746] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.122179] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e10000 to encoder DSI-34: -19
[ 2.133795] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 2.142069] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 2.149737] imx-drm 32c00000.bus:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.159410] [drm] Initialized imx-drm 1.0.0 20120507 for 32c00000.bus:display-subsystem on minor 1
[ 2.164411] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout
[ 2.173449] pps pps0: new PPS source ptp0

0 件の賞賛
返信
1 解決策
7,092件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I see that the "Can't find PMIC:PCA9450" I think it is the PMIC cause the failed boot.

Maybe the board in your hand is old board with the ROHM BD71847MWV, but our newest version board and BSP use and support PCA9450.

In your side Linux 4.14.98_2.0.0 work well, because this version BSP support the old design with the BD71847MWV.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
7,093件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I see that the "Can't find PMIC:PCA9450" I think it is the PMIC cause the failed boot.

Maybe the board in your hand is old board with the ROHM BD71847MWV, but our newest version board and BSP use and support PCA9450.

In your side Linux 4.14.98_2.0.0 work well, because this version BSP support the old design with the BD71847MWV.

0 件の賞賛
返信
7,087件の閲覧回数
faraz7321
Contributor I

Thank you for your prompt response!

I am using 2018 NXP iMX8MM-EVK LPDDR4 version of the board and thats why I cannot get the latest Linux distro on my board.

Thanks again!

0 件の賞賛
返信
7,082件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome.

If you want to use the newest BSP, you need to do the PMIC porting for your board.

0 件の賞賛
返信