I am looking to find the method, recommended by NXP, to successfully make a factory image of a nand chip for
manufacturing. The image, or images, should cover the entire chip and should be capable of being burned
directly to multiple nand flash chips in an assembly line. The nand chip is the Micron MT29F32G08CBADA. The
controller is the IMX6UL. The only method where I have successfully created a set of images and re-burned
them was using nanddump and nandwrite. But this process was done on the same board, using the same nand and SOM.
And this process is incompatible with our manufacturer.
Whenever I take those images and burn them to a different nand, using Dataman, it won't boot. The burner
I'm using is the Dataman-48Pro2. I have tried burning images, that have been pulled using nanddump that worked using the nandwrite method. I have also tried desoldering a working nand chip, reading the image off , burning that image to a new
chip and soldering that chip down. Nothing has worked.
Since kobs-ng is how the mfgtool writes uboot to nand, it seems the best place to start. According to it's output, kobs-ng
writes three sections for uboot: fcb(4 copies), dbbt(4 copies) and the bootstream ( 2 copies of uboot binary).
The sections dbbt and uboot seem to be treated similar in terms of OOB data. The fcb section, however, seems
unique in that it doesn't seem to use ecc.
The method I used to create a backup and re-write images to nand, that successfully boots, is below:
Read:
nanddump -o -n -f fcb.bin -s <start addr> -l <length> <device>
nanddump -o -f dbbt.bin -s <start addr> -l <length> <device>
nanddump -o -f bstream.bin -s <start addr> -l <length> <device>
Write:
nandwrite -o -n -s <start addr>  <device> fcb.bin   
nandwrite -o -n -s <start addr> <device> fcb.bin
nandwrite -o -n -s <start addr> <device> fcb.bin   
nandwrite -o -n -s <start addr> <device> fcb.bin
nandwrite -o -s <start addr> <device> dbbt.bin
nandwrite -o -s <start addr> <device> dbbt.bin    
nandwrite -o -s <start addr> <device> dbbt.bin
nandwrite -o -s <start addr> <device> dbbt.bin
nandwrite -o -s <start addr> <device> bstream.bin
nandwrite -o -s <start addr> <device> bstream.bin
One of our partners is using a TI arm based som. They have a working process using nanddump. The difference is that
we use the IMX6UL and it has the first boot function (xloader) embedded in it's rom where the TI arm doesn't. Is it possible
that the imx6 has a unique ecc algorithm that currently isn't supported by our burner?
This problem can't be new. Someone has to have solved the problem of creating a factory image for the IMX6UL using the
nand chip mentioned above. Does anyone know what NXP recommends for creating a factory image?
b36401, please continue with the follow up.
Thank you Karina and Victor. Victor replied with a follow up. Unfortunately, the files provided didn't indicate how to solve the problem of creating a factory image. Does anyone at NXP know what to supply to gang programmers to successfully create a bootable nand chip (similar to kobs-ng/mfgtool)? Are there companies that use the i.MX6
with raw nand that can burn their uboot to raw nand through 'some' chip programmer?
Unfortunately software ECC algorithm is not available.
Sorry for the inconvenience.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
When you say, "software ECC algorithm is not available", do you mean the ECC algorithm has not been made available to
chip burning manufacturers and therefore the mentioned manufacturing process cannot be done?
A am going to forward the question to our Experts Team.
However I need a case to point it in the form.
Please create a technical case:
https://community.nxp.com/thread/381898
Have a great day,
Victor
This was not answered and should not be considered answered.