Facing issue when flashing through USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Facing issue when flashing through USB

623 Views
shamiullah
Contributor III

Hello

I am using customized board based on NXP IMX6UL EVK board. There is a difference in the part numbers of SOC

----------------------------------------------------------------------

NXP IMX6UL  EVK Board       

Processor -- MCIMX6G2CVM05AA

---------------------------------------------------------------------

Customized IMX6UL Board

Processor --- MCIMX6G3CVM05AB

--------------------------------------------------------------------

The part numbers of USB, UART , RAM and eMMC are same The part number of RAM is

MT41K256M16TW-107 XIT:P and  eMMC is MTFC8GAKAJCN-4M IT TR(8GB Micron).  Used the same lines which are used in NXP EVK for eMMC , USB and RAM. I successfully flashed the NXP EVK Board using the UUU tool through USB. The same thing i replicated on my custom board. I am facing the following issue when i am trying to flash the custom board through USB using UUU tool. 

ERROR: HID(W) : LIBUSB_ERROR_TIMEOUT

Are there any differences in between MCIMX6G2CVM05AA and MCIMX6G3CVM05AB SOC's ? Do we have to make any modifications based on the difference of part numbers in SOC's ?

Please let me know if  any

 

Thanks & Regards

ShamiullahWhatsApp Image 2021-06-17 at 12.56.49.jpeg

 

 

0 Kudos
Reply
0 Replies