FUSE_PORx bits of MMPF0100.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FUSE_PORx bits of MMPF0100.

Jump to solution
1,152 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100.

MMPF0100 has FUSE_PORx bits , however there is no description about these bits in MMPF0100 datasheet (Rev.7.0).

Could you let me know the function of these bits?

Best Regards,

Satoshi Shimoda

Tags (2)
0 Kudos
Reply
1 Solution
1,012 Views
Yuri
NXP Employee
NXP Employee

Correct, any of the FUSE_PORx may be used, no difference between them.

View solution in original post

0 Kudos
Reply
3 Replies
1,012 Views
Yuri
NXP Employee
NXP Employee

OTP fuse bit FUSE_POR can be blown so that upon subsequent power cycles, the start-up sequence

is chosen from the OTP fuses and not from the TBBOTP registers.

1,012 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

Thank you for your reply.

Then, I want t to know the difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3 also.

I guess the start-up sequence is defined as below.

If this is correct, there is no difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3.

Is this right?

FUSE_POR.png

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,013 Views
Yuri
NXP Employee
NXP Employee

Correct, any of the FUSE_PORx may be used, no difference between them.

0 Kudos
Reply